(G2H) Guaranteed to Hold. Select Here for more information about G2H courses.
Model Based Definition using PMI, an exclusive offering by the Siemens US Training team, is designed for users who plan to use the Product and Manufacturing Information (PMI) application to add manufacturing and other information to a part model. You can attach information needed by downstream applications such as tooling, manufacturing, inspection, and shipping. The information can be text, dimensions, GD&T, or symbols.
Required courses:
Or
Successful completion of Essentials for Designers prerequisite assessment on the Learning Advantage (score >70%). Learning Advantage courses can also be used to prepare for the prerequisite assessment.
Working knowledge of the following:
For LIVE! classes, customers are required to have NX 11.0.1 installed.