The Active Workspace Declarative Customization course is a lesson extracted from the Active Workspace Customization & Configuration course, which will help Active Workspace developers understand the Declarative framework in Active Workspace, as well as learn how to build custom interface components using the Declarative framework. Students will setup a development environment and create custom components to deploy and test with the client.
The course walks students through a review of the installation directory for the Active Workspace Client installation directory and the required scripts / files needed to perform customization. Then the course progresses into setting up a development environment to allow for easy development cycles and testing. Finally, the course dives into the Declarative Framework and examples of developing in the framework utilizing the development environment.
This class is compatible with the following version(s) of Active Workspace: 3.3, 3.4
Teamcenter Customizers
Required courses:
For this LIVE! class, customers will use our cloud training environment, so no local software is needed.
A Siemens Xcelerator Academy account will be provided to each student for access to training materials.
Day 01
Course Overview & Introduction
Environment Review
Setup a Development Environment
Day 02
Create a Basic Command
Create a Global Command
Day 03
CTX Service Review and Utilization
Create a Global Command to Use Data from CTX
Additional Demos: Visual Indicators, CSS overrides, Locations