Calibre
Calibre Writing DRC/LVS Rules

Course Code
239707-CN
Software
Calibre 2026.2
Language
中文(简体)
User Level
All
Pricing ID
Select Country
List Price
Select Country
Price may not include taxes applicable to your billing region
Contact us for private event pricing
Live Online Duration
6 hours for each day for 8 days

The Calibre Fundamentals: Writing DRC/LVS Rules" course will teach you to effectively write and maintain Calibre nmDRC and nmLVS rule decks for your semiconductor processes. In this class, you will extensively study the Standard Verification Rule Format (SVRF) language used in Calibre rule decks.

PREREQUISITES

  • Completion of the Calibre nmDRC/nmLVS class is very highly recommended
  • Thorough knowledge of IC layout techniques and procedures
  • Experience with an IC layout editing tool
  • Good understanding of SPICE netlists
  • Familiarity with UNIX
  • Good understanding of layout verification concepts and experience with layout verification tools

PROVIDED COURSE MATERIALS
Class Package
Find Upcoming Classes
For more information
Learning Services, EDA China

PRIMARY COURSE TOPICS

You Will Learn How To

  • Write DRC rules that perform a full complement of layout dimensional checks
  • Write specification statements to control DRC output
  • Use Boolean and topological operators to derive new layer data
  • Debug rule files
  • Write polygon-directed and edge-directed checks
  • Write basic and enhanced antenna rule checks
  • Improve DRC run-time efficiency
  • Write equation-based DRC rule checks
  • Create and use layer properties
  • Reconcile rule file and layout precision
  • Write rules to establish layout connectivity
  • Write rules to recognize different devices such as MOS transistors, resistors, and capacitors of different types, bipolar transistors, etc. in the layout
  • Extend the set of built-in device templates to include your own custom devices
  • Extract various properties such as width, length, resistance, and capacitance of recognized devices, using the Built-in property language within Calibre nmLVS TM and compare these values with those specified in the source netlist
  • Effectively utilize the text present in the GDSII layout database, and supplement it with text supplied through the rule file to annotate nets and ports
  • Optimally use the various Calibre statements that deal with net and port names in the layout
  • Write various LVS specification statements that control how the layout netlist extracted from the layout database is compared to the source netlist

Hands-On Labs

Throughout this course, extensive hands-on lab exercises provide you with practical experience in using Calibre under the guidance of our expert instructors. Hands-on lab topics include:

  • Preparing the Rule File and Running Calibre
  • Viewing DRC and LVS Results
  • Using the Online Documentation
  • Writing Layer Definitions
  • Writing DRC and LVS Specification Statements
  • Writing and Testing Dimensional Rule Checks
  • Designing and Testing Derived Layer Statements
  • Writing Polygon-directed Rule Checks
  • Designing and Testing Edge and Error-directed Rule Checks
  • Creating and Using Layer Properties
  • Writing and Testing Connectivity Statements
  • Designing and Testing Antenna Rule Checks
  • Taking Advantage of Hierarchy
  • Setting LVS Report Options
  • Finding Soft Connections
  • Creating and Naming Ports
  • Inserting Text Objects Into a Layout Using the Rule File
  • Writing Device Recognition Statements
  • Specifying Custom User-Defined Devices
  • Using the Built-In Language to Define Device Properties
  • Writing TVF code to generate a DRC rule file