NX
CAD Advanced Processes

Course Code
TRCT2220
Software
NX 12.0
Language
English
User Level
Intermediate
Pricing ID
Select Country
List Price
Select Country
Price may not include taxes applicable to your billing region
Contact us for private event pricing
Live In-Person Duration
5 Days

The Advanced Processes course is designed to propel students further up the efficiency curve. As a second tier course Advanced Processes builds on the tools you deployed as a result of attending the NX CAD Fundamental Workflows course. The real-world experience of the Siemens instructors aids students in transferring knowledge gained through this single course to their job resulting in faster time to productivity.

At the completion of the Advanced Processes class, the student will be able to develop complex parametric solid and assembly models. This task-based process course focuses the student on productive modeling techniques that capture design intent in the context of the Master Model. These concepts can be applied in the real world of product development and collaboration. As with each course developed and taught by Siemens PLM Software professionals, this class reinforces our in-depth knowledge of the software's capabilities and instructs the students based on the underlying principles incorporated within the NX product suite. This class was designed to increase the productivity of the student, teaching the necessary skills to accomplish the following:

  • Apply advanced sketch constraints to capture design intent
  • Use basic surfacing techniques to build parts
  • Develop models to support manufacturing processes
  • Translate and modify non-parametric model data
  • Use top-down assembly modeling technqiues to establish interpart relationships
  • Build assembly configurations using arrangements
WHO SHOULD ATTEND
  • This course is for designers, engineers, and CAD/CAM managers who need to create parametric solid models that capture design intent.
PREREQUISITES

Required courses:

Or

  • Successful completion of Designing Parts in NX prerequisite assessment on the Siemens Xcelerator Academy (score >70%). Siemens Xcelerator Academy courses can also be used to prepare for the prerequisite assessment.

PROVIDED COURSE MATERIALS
  • Student Guide
  • Activity Material
ATTENDANCE REQUIREMENTS
This course was written against NX 12.0.1

For LIVE! classes, customers are required to have NX 12.0.1 installed.

Find Upcoming Classes
For more information
Learning Services, Brazil

PRIMARY COURSE TOPICS

Day 1

  • Modeling basic parts using surfacing techniques
  • Controlling design intent using conditional formulas
  • Adding advanced features to molded and cast parts

Day 2

  • Starting a model using imported CAD data
  • Building parts with duplicate geometry
  • Displaying and analyzing assembly structures

Day 3

  • Modeling parts in the context of an assembly
  • Linking geometry between related component parts
  • Creating expression links between parts

Day 4

  • Preparing models for down-stream manufacturing processes
  • Duplicating components using patterns
  • Working with and defining reusable part data

Day 5

  • Cloning assembly structures
  • Editing and revising assembly structures
  • Configuring an assembly using arrangements