Course Description
NX
CAD Surface Modeling Processes
With Teamcenter Integration
With Teamcenter Integration
Class is taught in the Teamcenter integration environment using Active Workspace embedded in NX.
The Surface Modeling Processes course is designed to cover the process of how to create freeform parts that update reliably and shift smoothly to the manufacturing application. As a second tier course Surface Modeling Workflows builds on the tools you deployed as a result of attending the NX CAD Fundamental Workflows course. The real-world experience of the Siemens instructors aids students in transferring knowledge gained through this single course to their job resulting in faster time to productivity.
At the completion of the Surface Modeling Processes class, the student will be able to incorporate freeform features into any part, from product models to complex engineering designs. This task-based process course focuses the student on productive surface modeling techniques that capture design intent. These concepts can be applied in the real world of product development and collaboration. As with each course developed and taught by Siemens PLM Software professionals, this class reinforces our in-depth knowledge of the software's capabilities and instructs the students based on the underlying principles incorporated within the NX product suite. This class was designed to increase the productivity of the student, teaching the necessary skills to accomplish the following:
- Create splines and derived curves used in creating freeform features.
- Analyze curves and faces.
- Build primary surfaces using curves.
- Create freeform shapes by sweeping sections along curves.
- Create transition and blend shapes.
- Extend and offset surface geometry.
- Convert surfaces into solid models.
- Add draft to molded and cast part models.
- Deform parts using Global Shaping.
- Engineers and designers that need to create, edit, and analyze curves and freeform shapes used in part design.
Required courses:
- CAD Fundamental Processes (TRCT2205-TC)
Or
- Essentials for NX Designers (TR10051)
- CAD FastStart for Experienced 3D CAD Users(TRCT2210-TC)
- Successful completion of Designing Parts in NX prerequisite assessment on the Siemens Xcelerator Academy (score >70%). Siemens Xcelerator Academy courses can also be used to prepare for the prerequisite assessment.
-
Other recommendations:
- NX domain knowledge
- NX modeling and sketching
- Student Guide
- Activity Material
For LIVE! classes, customers are required to have NX 12.0.1 installed.
PRIMARY COURSE TOPICS
Day 1
- Introduction to surface modeling processes
- Using 3D curves as construction geometry
- Creating freeform shapes from splines
Day 2
- Using mesh surfaces to define primary features
- Styling shapes to build sculpted surfaces
- Sweeping sections to start a design
Day 3
- Building exact geometry to define irregular shapes
- Overbuilding and combining surfaces to build a part
Day 4
- Defining transitional geometry between shapes
- Analyzing the quality of freeform geometry
Day 5
- Using surfaces to add definition to a solid model
- Deforming surfaces for manufacturing processes
- Optional: Working with raster images
- Optional: Introduction to reverse engineering